Part Number: TPS65987D
Other Parts Discussed in Thread: TIDA-050012, TPS65981, ,
Using the TPS65981 Application customization tool, I tried to program the TPS65987DDH/Standard/Downstram Facing Port/ configuration onto the TIDA-050012 DUO Source Board. It should then behave like the TPS65987DJEVM board i.e. i should not have to press any of the configuration buttons. But the board still works as if it is programmed with the default configuration. I know the configuration tool gives me error free messages when I am downloading.