Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB953-Q1, , DS90UB934-Q1
Hi :
My question is similar to following link. Due to certification regulations, I must isolate between 954 and 953.
In the first answer, TI's engineer (Steven) mentioned a sentence "while FPD-Link selects NRZ modulation".
I looked for the datasheet of 953 & 954, I did not find the relevant explanation.
But there is an Encoder in the 953 system block diagram and a Decoder in the 954 system block diagram.
I want to further confirm whether FPD-LINK has NRZ encoding? Are these Encoder and Decoder the NRZ processing unit?
I want to continue the questions asked by the previous web-link. I only need to find a transformer with a higher bandwidth (eg >4Gbps / per-pair)
FPD-LINK can be designed in isolation, right?
Best Regards
Denis