Hello, my customer is using the TPD3S014 in an application, where at the start of the application the input voltage can raise up to 6V – just for a short period of time.
After that, the device works 24/7 all day/night. So during lifetime of TPD3S014 it will see only few of those events.
The Enable pin is low in this event.
Can you please elaborate on technical details if / how you would allow such kind of condition?