Part Number: TUSB546A-DCI
Other Parts Discussed in Thread: TUSB546-DCI
Dear TI engineer.
I have a question about TUSB546A usage.
<Our status>
- dp 2 lane + usb3.0 2 lane
- Do not use HPD pin (using PD VDM message)
- TUSB546 I2C mode usage
1. General register setting
EQ_OVERRIDE = 1
HPDIN_OVERRIDE = 1
Q1. Is it correct to set the register with above value?
Q2. When set to HPD_IN is high, what does TUSB546 do?
2. Link training
Q3. When Displayport dongle is connected, is it correct to set CTLSEL to 10 (4 lane DP) / 11 (2 lane DP + USB3.1)??
Q4. Link training fail does not occur in Apple multiport dongle (simultaneous support for HDMI / USB / Type C), But, ordinary Displayport dongle (HDMI only), Link training fail is occurring.
Do we have to do more setting for TUSB546 register??
3. Aux snooping mode
If using TUSB546-DCI in I2C mode, then system software must disable AUX snooping whenever the CONFIG1 pin is high. (from specification document)
-Current Aux snooping mode is on, and CONFIG1 (CAD_SNK) Pin is not connected.
Q5. Is it correct to turn on Aux snooping when I2C mode, when CONFIG1 (CAD_SNK) Pin is not connected?