Part Number: DS90UB954-Q1
Hi team,
We are using DS90UB954 to deserialize DS90UB933, DS90UB933 receive data format is YUV422 8Bit(UYVY). Now both Lock and Pass of DS90UB954 are high level, 0x5b register(SER_ID ) can also read to 0xB0,but 0x75\0x76 register(LINE_LEN_1\LINE_LEN_0) different from actual.Why does this happen?
It is known that 933 works fine on other platforms.
Our configuration for 954 is as follows:
MODE PIN:1.8V
Register:
0x33, 0x01
0x0C, 0x81
0x4C, 0x01
0x20,0x20
Do we need to do other configuration to decode normally?
Best regards,
Alec Li