Part Number: TUSB320EVM
Other Parts Discussed in Thread: TUSB320, TPS2121, TPS63020, TPS25910
Hi All
I'm currently evaluating the TUSB320 for a USB Type C project, when looking into the evaluation board schematics I can see Oring power through RB751V-40 diodes, they are highlighted in the screenshot below.
The Datasheet of those diodes mentions current rating of 30mA only.
I was wondering how this could work since the board is rated for 3.0A, while the diodes are only supporting 30mA ?!
Where am I wrong ?
Thanks