Part Number: TUSB1002A
Other Parts Discussed in Thread: TUSB1002,
Hi Sir,
if TUSB1002A can replace TUSB1002?
And this is our circuit of TUSB1002A? but it can not transfer data, would you pls help us check the sch?
thanks.
BR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
make sure EN pin to high, Mode is floating.
replace C3 C4 C5 C6 to 330nf.
yes, TUSB1002A can replace TUSB1002. A version fixed some bugs in no -A version.
To setup EQ and CFG, pls look at section 8.2 in datasheet. If you still have question, let's discuss in email.
1: redefine pin 14
2: fixed RX termination to Gnd
3:reduce power in low power state.