Other Parts Discussed in Thread: SN74CB3Q3253, TMUX136
May I know if TI has p2p or similar part?
1. PI3USB14-AZHE: IC OTHER (20P) PI3USB14-AZHE TQFN
2. PI3USB103ZLE: IC OTHER(10P) PI3USB103ZLE(TQFN)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74CB3Q3253, TMUX136
May I know if TI has p2p or similar part?
1. PI3USB14-AZHE: IC OTHER (20P) PI3USB14-AZHE TQFN
2. PI3USB103ZLE: IC OTHER(10P) PI3USB103ZLE(TQFN)
Hi Jazz,
We don't have a p2p for the parts you have listed above. However, we do have products that are similar. See below.
1. PI3USB14-AZHE vs SN74CB3Q3253.
| Diode | TI | |
| Family | PI3USB14-A | SN74CB3Q3253 |
| PN | PI3USB14-AZHEX | SN74CB3Q3253RGY |
| Configuration | 2 Channel 4:1 MUX | 2 Channel 4:1 MUX |
| Supply Voltage | 3.3V Operation | 2.3 - 3.6V |
| Propagation Delay | 0.3 ns | 0.18 ns |
| Ron | 4.0 Ω (typ) | 4.0 Ω (typ) |
| BW (-3dB) | 815 MHz | 500 MHz |
| OFF Leakage Current | < +/- 2 µA | < +/- 1 µA |
| Package | TQFN - 20-pin Very Thin Quad Flat, No Lead (TQFN) (3.5mm x 4.5mm x 0.75 mm) | VQFN - 16-pin Very Thing Quad Flat, No Lead (VQFN) (3.5mm x 4.0mm x 0.9 mm |
| Notes | Wider Bandwidth | Lower OFF leakage current, Lower propagation delay |
2. PI3USB103ZLE vs TMUX136. The TMUX136 has wider bandwidth and has charge pump.
| Diode | TI | |
| Family | PI3USB130 | TMUX136 |
| PN | PI3USB103ZLE | TMUX136RSER |
| Configuration | 2 Channel 2:1 SPDT | 2 Channel 2:1 SPDT |
| Supply Voltage | 2.7 - 4.2V Operation | 2.3 - 4.8V Operation |
| Propagation Delay | 0.25 ns | 0.10 ns |
| Ron | 3.0 Ω (typ) | 5.7 Ω (typ) |
| BW (-3dB) | 1.5 GHz | 6.1 GHz |
| OFF Leakage Current | < +/- 2 µA | < +/- 2 µA |
| Package | 10-contact, Thin Fine Pitch Quad Falt No-Lead (TQFN) Package (1.3mm x 1.6mm x 0.75mm) | Compact 10-Pin UQFN Package (1.5mm x 2mm, 0.5mm Pitch) |
| Notes | Lower Ron | Includes Charge Pump, Wider Bandwidth, Lower Propagation Delay |
Thanks,
Jon