Part Number: SN65LVCP114
If I understand correctly, the SN65LVCP114 can be put in diagnostic mode and split a 6Gbps signal. Just to make sure I am clear, I need to split the signal (one input, two simultaneous outputs) and not simply mux the signal. Are there any concerns in making the device to permanently operate in diagnostic mode? What are the limitations, concerns, or issues with releasing a product based on this feature?
Thank you!