Part Number: TPS65988EVM
Other Parts Discussed in Thread: TPS65988, TUSB8020B, HD3SS3212
HI
This is Sridharan.
We are Designing an Adapter Module Operates with a 5V Supply External and has two USB type c port
1. one for USB DRP (host/sink) - USB Plug
2. one upstream facing port (USB dongle or mass storage device). - USB device
We have chosen TPS65988 USB Type C Power delivery 3.0 controller used to provide simultaneously charge the Host as Source Sink mode and allows for data transfer from the Host through an external USB-C device.We using the Intenal Ath for both source (5V @2A) and Sink
We have a chosen TUSB8020B USB Hub to use with controller , We also need to terminate USB2 D+/D- signals.
We dont have schematics file though we have arrived at architecture from EVM guide. Kindly let us know if this would suit our requirements
Thanks and Regards
Sridharan