Part Number: ONET1130EP
Hi,
We are an electronics development company and we are developing a product for a client to convert electrical signals into optical signals at a frequency of 5Gbps.
The signals to be transmitted are a personalized signal with a squelch state which lasts between 5us and 1ms. How do the "TxOut" outputs of the ONET1130EP chip behave when the "TxIn" signals are squelched (V (TxIn +) = V (TxIn-)) ? Is the output undefined or the ONET1130EP can also squelch the signals if the voltage difference of the TxIn inputs is less than a certain threshold?
Thank you in advance for your answer.