Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9555: May TCA9555PWR can direct replace MAX7311AUG?

Part Number: TCA9555

Hi Sir 

I use cross reference to search MAX7311AUG replace part and find TCA9555PWR are P2P.

May TCA9555PWR  can direct replace MAX7311AUG? or something i need to remind my customer?

                                                                   Bogey

  • Hey Bogey,

    The two devices do look to share some similarities however I do notice two major differences.

    1) The register map for the MAX device has 2 additional registers for timeout and factory reserved register.

    2) The MAX device has more address options than our device

    -This may be an important detail which means depending on how the customer schematic is set up, our device may not be a suitable replacement. If you have a schematic/block diagram you can share of the specific socket we are looking to replacing then I can help you to confirm/deny this.

    -Bobby

  • Hi Bobby 

    Since TCA9555 can't be use, may you have other suggestion part?

                             Bogey

  • Bogey,

    TCA9555 would be as good of an option as anything else here.  None of our IO expanders have a bus timeout feature or this many programmable address bits.  Can you please find out if these are really needed in this application?

    Regards,
    Max