Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Hi team,
Customer is considering to use DP83869HM as a SERDES for 1000BASE-T.
Is it possible to relay 1000BASE-T between two DP83869HM without fiber transceiver?
Two DP83869 is going to connect with co-axiial cable with AC-coupling. The system under consideration is like below.
1000BASE-T system - 4 lines (1000BASE-T) - DP83869HM - 2 lines - DP83869HM -4 lines (1000BASE-T) - 1000BASE-T system
Also, Cusomer is considering to use DP83867 for the same purpose. The system is like below.
Is it possible to communicate between DP83867 with AC-coupling by SGMII(4wires)?
1000BASE-T system - 4 lines (1000BASE-T) - DP83867 - 4 lines - DP83867 -4 lines (1000BASE-T) - 1000BASE-T system
Regards,
Saito