Part Number: TCA6507
Hello expert,
Customer is asking if TCA6507 could support 1kHz PWM dimming for LED. They will need 3 set for 1kHz PWM on output. Could you kindly help to comment on it? Thanks a lot!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Max
Because We use PWM to our RT8511BGQW IC for Heater solution.
As we known, RT8511BGQW could use PWM frequency from 100Hz to 8KHz.
Until now,our test always use 1KHz PWM to push 150 mA current.
So we hope 1KHz could be push from TCA6507.
Thanks!
Thank you for the clarification; I understand. Unfortunately such a high frequency isn't possible with TCA9507, but since RT8511BGQW can work with 125 Hz at least it is possible to try this lower frequency. If you find that you need the higher PWM frequency there are other methods for generating PWM waveforms you can find at the resources below.
http://www.ti.com/lit/ug/slau508/slau508.pdf
http://www.ti.com/lit/ug/tiduc97a/tiduc97a.pdf
Regards,
Max