Part Number: TFP410-EP
Other Parts Discussed in Thread: TFP410
What is the use of I2C pin ?
TFP410 doesn't require configuration/initialization (through I2C) unless we want to enable the DE generator
What exactly is DE generator ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shekkhar,
The DE generator is for if the video source does not have a DE signal, which is required for display panels.
Regards,
I.K.
Hi Shekhar,
It is better to ask your questions here so that other people that may have the same question can see them.
Regards,
I.K.
Hi Sir,
I have TFP410 interfaced with Zynq UltraScale+ chip.
So, my video source is the Zynq, So will this have a DE signal ?
Else we need to configure through I2C, If then, could you please provide i2c software .c file for below specification ?
RES = 720x480p
Blanking = 25%
Hi Shekhar,
You'll need to check with Xilinx or go through that chip's datasheet to confirm whether or not it has a DE signal.
Also, we don't provide code for the TFP410. Since the configuration is only through pin-strapping or I2C, you can go through the register map or pin descriptions in the datasheet and check what settings you need to configure.
Regards,
I.K.
Hi Sir,
Thank you for your inputs.
The TFP410 requires a reset after power up, so if i do reset i.e SEL/RST# low to high, then I2C is selected and chip configuration is set based on the configuration bits (BSEL, DSEL, EDGE) and state bits (PD, DKEN) in the I2C registers
Now I have to configure the I2C registers for my 24bit, single-edge, rising, single ended clock mode.
Then what is the use of hard-wiring on boards these pins, which are of no use when I power cycle [OFF -> ON] ?
Hi Shekhar,
Please see the descriptions for these pins in the Pin Functions table in the datasheet. It describes their use when I2C is enabled/disabled.
It's a lot easier to configure the device through pin-strapping rather than through I2C, so I recommend verifying whether or not your source generates DE.
Regards,
I.K.
Hi Sir,
So as far i understand, below is the functional sequence [assuming SCH is correct]
Please provide your feedback on our approach
PS: Soon shall share with the I2C register values for DE generation
That looks okay. Don't forget to set the polarity of HSYNC/VSYNC in DE_CTL.
Regards,
I.K.
Hi
Actually I got to know that we are generating DE Generator from our Zynq FPGA
Sowe shall only use ISEL/rst for power on reset and then pull it down for pin strapping.
Still do we need to configure few resistors via I2C ??
Hi Shekhar,
No, you don't need to use the I2C interface if your FPGA is generating DE.
Regards,
I.K.
Hi
Thank you, but how come the chip knows my HSYNC, VSYNC polarity
And If I need DDC signals to the DVI Monitor from this chip, how shall I interface?
Hi Shekhar,
Sorry for the delay. The TFP410 does not interface with DDC, so it will need to go straight from your source to the DVI monitor.
Regards,
I.K.