Part Number: DP83867IS
Hi,
We have a custom board designed with xilinx Zynq Ultrascale+ FPGA. We have connected it to two ethernet ports. 1 port operated using SGMII(4 wire) interface and the other through RGMII. PHYs used are the same(DP83867ISRGZT). When I connected the port on RGMII to the PC(capable of 1GBps) I see 1 gigabit link is established. But the same does not happen with SGMII connected port. It always downshifts the link to 100mbps. I need to mention here that SGMII was still able to establish 1gigabit connection on few other ports but it is very selective. SGMII failed to establish 1GBps link on some of the ports where RGMII was able to. Could you please let me know what could be the issue and how to solve it/debug it?
Thanks in Advance and Best Regards,
Arjun