Part Number: PCA9306
Hi Everyone,
currently I'm working with a 1 MHz i2c-bus. The high level output of the master is at 1.25 V, but the slave needs at least a level of 1.4V to recognize a high level.
The slave is powered by a supply voltag of 1.8V. For this reason i was looking around for i2c-Bus level shifters. The PCA9306 was almost perfect with a minimum voltage VCCB of 1.8 V , except for the maximum frequency of 400 kHz.
I was wondering if there is an updated version, which can work wih 1MHz i2c-connections, ore another product that suits my requirements, but i wasn't able to find.
Thx in advance and have a nice day.
Best Regards,
Lukas