Part Number: TRS3253E
Dear Sir
I have a application need RS-232 level converter for 3T3R, and the logic level is 1.8V.
I have two question.
1.
Could I connect the logic signal of 1.8V to TRS3253E directly? Or I still need a level shifter(1.8V to 3.3V ) between logic signal and TRS3253E?
If I can connect with TRS3253E directly, I need set the VL=1.8V, right?
2.
I only have 3.8V on board, could I set the VCC as 3.8V? Or I must need to generate another voltage of 3.3V as VCC?
Thanks.