Other Parts Discussed in Thread: TPD1E01B04
Hello All,
I want to hardened USB ports in an uncontrolled ESD environment e.g., office environment. Additionally, I don't want the user to have to wear a ESD wrist strap when plugging in the USB cable, i.e. I don't want to label the port with an RS-471 sticker! Will this IEC 61000-4-2 8 kV provide sufficient protection?
In the literature I've been reading, IEC 61000-4-2 only tests in the powered state when the system is operational and looks for soft faults. However, i'm also concerned with damage when the equipment is in an unpowered state and any hard faults that may be associated with that. It seems an ESD path in unpowered vs. powered state can vary widely. Will the TPD1E0B04 provide sufficient ESD protection when the equipment is in both unpowered and powered states?