This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410: TFP410

Part Number: TFP410

Dear Sir

We are trying to get an image out of the TFP410 without success for now.

We supply the TFP410 currently with the following resolution specifications :

Resolution 640x480 with 60fps and pixel clock of 25.175Mhz

Horisontal front porch : 16

Horisontal sync             : 96

Horisontal back porch : 48

Horisontal Total           : 800

Vertical front porch     : 11

Vertical sync                   : 2

Vertical back porch       : 32

Vertical Total                 : 525

 

The TFP410 pin settings are :

EDGE – '0'

PDn   - '1'

ISEL   - '0'

DSEL   - '0'

BSEL   - '1'

RESERVED – '0'

DKEN   - '0'

TFADJ - 510 Ohm

Roi