Part Number: AM26C31M
Other Parts Discussed in Thread: THVD1500, AM26LV31
Hello, I need to know the active output impedance of the following parts:
AM26C31MDREP
AM26LV31ESDREP
The datasheet does not state in either case.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The driver's impedance is not linear. In RS485/422 systems, if the bus is terminated properly at the receiver side, the reflection should be minimized and the driver side won't see much energy bounced back. You can refer to this blog for the discussion about termination.
Regards,
Hao
Do you have any detailed I vs. V curves for the AM26LV31ESDREP?
We are considering a series-terminated application, RS-422 (so one transmitter, one receiver). This application has no DC current, though there will be a brief but small pulse of AC current to charge the cable capacitance. We are controlling impedance to 100 ohms, differential. Can you recommend a value of series termination resistor to use?
Also I think there may be a typo in the app note:
IS: One situation in which you don’t need termination networks is when the two-way loop time of the network is much greater than a single bit time (~<0.1×two-way loop delay). In such scenarios, the reflections will lose energy each time they reach an end of the network.
SHOULD BE:
One situation in which you don’t need termination networks is when the two-way loop time of the network is much less than a single bit time (~<0.1×two-way loop delay). In such scenarios, the reflections will lose energy each time they reach an end of the network.
It might take some time to generate the output voltage vs. current curve of AM26LV31. I'll get the data for you.
About the point on the blog, I think it meant the reflection energy will die out traveling in the long cable. On the other hand, if the distance is short, the impact could be observed at the transmitter output, for example a step at the rising edge. This app note is a good resource for the technical discussion about reflection.
Regards,
Hao
I'll stay tuned for the data and your recommendation.
I see your point on the blog post; I was looking at this from the perspective of critical length which indicates a maximum cable length, given a driver's risetime. An unterminated connection shorter than the critical length may have reflections, but they will die out before the signal settles out to its new value. This notion assumes the reflections at the receiver are too small to cross logic thresholds & generate glitches.
Josh