Part Number: TIR1000
Other Parts Discussed in Thread: TL16C550C
Hi,
In a design we are planning to implement IR Data transmission (Transceiver) at lower speed maximum of 115200 bits/second. I found this part TIR100 can do the Job but I have few doubts as follows
- In datasheet it is mentioned that 16Xbaudrate clock must be used which means here i have to use 1.8432 Mhz should be used is that correct? Or we can use higher clock than this like 2 Mhz or 8Mhz?
- Is that RX and TX indicates UART protocol which can be connected to a micro controller directly? or do we need other PHY like TL16C550C which was mentioned in datasheet ( http://www.ti.com/lit/ds/symlink/tir1000.pdf?&ts=1589729902497 Page 9)