Part Number: DS90UB954-Q1
Hi team,
We now have a project on DS90UB954,the chip at the next level needs to be configured with these parameters to decode correctly.The chip in the next level has a range requirement for these two parameters, so we want to reconfigure it.
Now,we have three questions to ask:
1.What are the units of device DS90UB954 register CSI0_THS_PREP(Indirect Address Page 0x00; Register 0x44) &CSI0_THS_ZERO(Indirect Address Page 0x00; Register 0x45)?
2.If i set the register CSI0_THS_PREP =0x86/CSI0_THS_ZERO = 0x8c, what is the actual Ths-prep/Ths-zero output?
3.Are there any points to note when setting CSI0_THS_PREP & CSI0_THS_ZERO or need to cooperate with setting other registers?
Best regards,
Alec Li