Part Number: DS25BR440
Does ~PWDN 0/1/2/3 pin requires pull up/down resistors when driving by a logic output driver?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS25BR440
Does ~PWDN 0/1/2/3 pin requires pull up/down resistors when driving by a logic output driver?
Hi,
The pins accept a LVCMOS input signal directly, for normal operation no resistors would be needed. Depending on the application and system it may be useful to have a pull-down resistor connected to the PWDN pins. This will ensure that the DS25BR440 will not output signals even if the logic device loses power.
Regards,
Lee