Part Number: TUSB8043
Hi,
I have planned to use TUSB8043 in my design. In datasheet I could find two temperature as
- Operating free-air temperature as 0 to 70 °C
- Operating Junction temperature as -40 to 105 °C
1.Can you let me know what is the difference between them?
2.And what will be operating temperature range of the device?
My design requirement for operating temperature range is -20 to 85 °C. Please confirm if I can use this device for my requirement
Thanks,
Menaka