Part Number: TPS65981EVM
Other Parts Discussed in Thread: TPS65981
I have a question about a potential system configuration using two TPS65981 devices. I need each side of the device to perform both source and sink functions. The system-side sources DP and sinks USB, while the host (PC)-side sinks DP (to be connected to a display) and sources USB. I have attached an edited version of Figure 5 from the TPS65981EVM user manual to illustrate the system. Is this configuration possible with the TPS, or can one TPS device only source or sink both types of signals?