Part Number: DS90UB960-Q1
Hi,
I have 4x1080p YUV2 camera attatched to on DS90UB960,and output via one CSI-2 port.
1.according to CSI-2 port speed, I have calculations as follow:
total data rates it can transmitted: 4x1.6Gbps = 6.4G bps
considering blank time of MIPI, we use 6.4G bps x 0.75= 4.8 Gbps for raw image bits.
2.Regarded 4x camera, we have
total data rates: 4 x 1920 x 1080 x 16 x Camera Framerate
so we have maximum Camera framerate = 36.16 fps
I have two questions here,
(1) If my calculations is right?
(2) Is it OK for DS90UB960 paired with 4x1080p YUV 30fps camera?
(3)In datasheet, DS90UB960 Supports 2-Megapixel Sensors With Full HD 1080p Resolution at 60-Hz Frame Rate.
Is this (1080p 60fps) real maximum capacity of DS90UB960 instead of 6.4G bps (this datarate will be 1080p YUV2 120fps)