Part Number: TUSB3410
Hi,
Previously from this forum I received an IrDA firmware for TUSB3410.
However, depending on the Linux environment used, it worked or not.
Using TUSB3410 as UART without EEPROM was fine in any environment.
PC/Ubuntu20.04 LTS with Linux 5.4
-> IrDAFW ok, noEEPROM(UART) ok
PC/Centos8.1-1911 with Linux 4.18.0-147
-> IrDAFW ok, noEEPROM(UART) ok
Tablet(MediaTek MT8167B)/Android8.1 with Linux 4.4.95+
-> IrDAFW fail(/ dev/ttyUSB is not generated), noEEPROM(UART) ok
Is there any limitation on the Linux kernel version when writing IrDA FW to EEPROM and using it?