This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: USB to SD card

Part Number: TUSB9261


Hi,

My customer is going to have a project with TUSB9261.

The following is the info they provided:

    For standard UFI command(or SCSI Commands) defined for USB Mass Storage Class, the bridge IC process them as usual.

    But for some specific commands,the bridge IC will pass/get the payload to/from the micro SD Card via 1-bit or 4-bit SDIO interface. (1-bit is enough, but 4-bit better)

    The SDIO interface of bridge IC can be implemented by GPIO using software/firmware in this design.

Please help to check :

1. If it is achievable by modifying TUSB9261 FW?

2. Does it have any SW or HW limitation for this application? 

Thanks.