This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401A: Unsteady output pixel clock with no signal input

Part Number: TFP401A

Ive gone through several board iterations trying to solve this issue. When no input hdmi signal is present the odclock pin randomly switches from high to low. It only does it when the heat pad is soldered, grounded or not, when not soldered i do not see the pulse on the clock at all, the result is a white halo on a lcd screen after being disbaled for about ten minutes. Once powered cycled and signal presen the lcd will heal. When not soldered this issue does not occur regardless of no signal duration.