Part Number: TPD12S521
Hi Guys
Please find my schematic about the HDMI Redriver and ESD sction.
Schematic:
About the HDMI classifacation test. the standby test. They need powet off the HDMI device and the equipment. And add a 3.3V(50ohm pull up) on the TMDS signal wire, and then test the signal voltage y using DMM. The requirement is 3.3V +/- 10mV. But so far they just got 2.6V. So how to solve this problem? Or did we meet the same quesiton before?
Please pay attention the attachment about the classificaiton test about the Voff test.
HDMI Classifacation requirement:
Your feedback are very appreciated.
Thanks
-Pengfei