Part Number: DP83867E
Hi,
What is the internal pull-up and pull down resistor values of DP83867E component?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
9K +/- 25% (part to part variation).
--
Regards,
Vikram
I would like to start the PHY at powered down status and let my FPGA decide to enable it.
As far as I understand, after power-up these pull-up on Interrupt/ Power-down pin will be disabled.
Until that time, there will be a conflict on this pin because it will be pulled down, externally and pulled-up internally.
To beat the internal pull up I need to place a smaller value resistor to pull it down. Do you have any recommendation for this?
Best Regards,
Onur
Same question is valid also for reset pin. It has an internal pull up but I would like to connect a pull down resistor to reset pin to keep it at reset state until FPGA release the reset. Any blocking item for me to add a pull down by default? and any resistor value recommended?
Best Regards
Onur
Hi Onur,
Sorry for the delay. I am discussing the constraints internally and will get back to you by 12th June.
--
Regards,
Vikram
Hi Onur,
After power up of the phy internal pull ups of 9K on pwdn and resetn pins are always enabled. So if you put a pull-down to make these inputs low, they will always stay low. Can you put an active switch to drive the level low of these pins when you want to keep them low?
Phy will power up fine in Rgmii mode and you need not write a regiter for sgmii or rgmii mode. But there is a note in datasheet which mandates the strap on rx_cntrl pin : See table 5 : 4-level strap pins. If you dont have the required strap then you need write a register as mentioned in the note below table 5.
--
Regards,
Vikram
Hi,
I saw it in the data sheet. But as far as I understand this is valid for only SGMII interface. Should I also put this strap pins to RX_Control pin for RGMII interface?
If it is valid and recommended for both RGMII and SGMII interfaces then I prefer to add these resistors to RX_Control pins.
Best Regards,
Onur Kusakoglu
Hi Onur,
I will re-check and confirm if it is only applicable to Sgmii mode. Did you see it any app note that strap on rx_ctrl can be ignored if in sgmii mode?
--
Regards,
Vikram
Please do the required register write( if not using rx_cntrl strap resistor ) for both sgmii and rgmii mode.
--
Regards,
Vikram