Part Number: TUSB522P
Hi expert,
For the re-driver model (TUSB522P)
1.Is the Rx model(file name : RX_generic.ibs) included cable model and CTLE? Or, I should implement the 3-m cable model and CTLE by myself at the end of the channel?
2. When I do the simulation, should we need to consider any PCH effects(ex: CPU package , buffer, pad loss)?
3.What’s components is inside the dB loss?(ex: CPU package , buffer, pad loss) or only PCB loss for -10.5 dB ?