This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: Lock signal during pattern generator output

Part Number: DS90UB936-Q1


Hi team,

My customer want to output black screen by pattern generator on UB936 during unlock and, recover the camera signal output once relock to the FPD Link input.

The Lock output is independent from pattern generator function, right?

Regards,

  • Hello Atsushi,

    Yes, LOCK and pattern generation are independent functions within these devices. There is no automatic method to start pattern generation when lock drops, but this could be implemented through system SW using an interrupt for example to signal the host to program the 936 into pattern generator mode.

    Best Regards,

    Casey