Part Number: TPS65988
Hi,
We are designing a system with Dual Port Type C USB. USB PD charger is planned to be connected to Port 1 whereas a battery powered device will be connected to Port 2.
The following are the use cases: 1. When the device is connected to the Port1 and no charger is connected in Port
1. the Power transfer is from VBUS2 to PPHV2 (act as a SINK) and then to the Buck to Power up the system.
2. Once charger is connected to Port1, then Port1 should be configured as SINK and request for a role swap of Port 2 as SOURCE and the Power transfers from VBUS1 --> PPHV1 --> PPHV2 --> VBUS 2. Also, it is branched after PPHV1 to supply the system.
3. Also, when the charger is disconnected from Port 1, a role swap request should be raised to configure the Port 2 as SINK again and draw power from the battery powered device.
Here, both the Port voltages are at 5V. Can the Role Swap (FRS) be achieved without any interruption to the System power supply?