Part Number: TPD2EUSB30
Can TPD2EUSB30DRTR be used for USB2.0 connector
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD2EUSB30
Can TPD2EUSB30DRTR be used for USB2.0 connector
Hi Jazz,
The TPD2EUSB30 has a low capacitance of 0.7pF in the DRT package and 0.8pF in the DQA package. These low capacitance will allow the device to operate with the USB2.0 data speeds without affecting signal integrity. To verify you can look at the insertion loss graph in section 6.6 typical characteristics where for USB2.0 data speeds(480Mbps) the insertion loss would be 0dB.
This device also offers level 4 IEC 61000-4-2 contact ESD protection, and 5A IEC 61000-4-5 surge protection capabilities.
Best regards,
Andy Robles