This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS80PCI800: VOD maximum

Part Number: DS80PCI800

Hi team, 

Datasheet mentions that DS80PCI800 can transmit VOD up to 1300 mVp-p. But it also referred that VOD control can be up to 1.4V.

I am confused, 1.3V or 1.4V, which one is VOD maximum?

  • Hi Miranda,

    The datasheet maximum VOD setting is 1.4V as you have highlighted in the SMBus register control field.  The typical VOD while programmed to be 1.4V is actually slightly lower.  The text information references the slightly lower voltage available in the highest output setting.  Typically it will be 1300 - 1350 mV.

    Regards,

    Lee