Part Number: DS90UB936-Q1
Other Parts Discussed in Thread: DS90UB954-Q1, DS90UB953-Q1
Hello,
Here is the title for DS90UB936-Q1" Dual 3 Gbps FPD-Link III Deserializer Hub With MIPI CSI-2 Outputs"
But, in the datasheet ,7.4.1, it says that "In CSI-2 mode each deserializer Rx Port can support an FPD-Link line rate up to 4.16 Gbps"
Which is correct? or any other meaning?
Also, In 935 datasheet, according table6, CSI bandwidth <= fx128=3.2Gbps which is different from the spec. which one is correct?
according this information ,I guess that 935 936 fpdlink work at line rate fx160 = 4Gbps, is it corrrect?
best regards
Nick Li