Part Number: XIO2001
Other Parts Discussed in Thread: LMK00334
Hi TI,
When refclk of XIO2001 is driven by a HCSL differential clock, what termination scheme shall be used?
When driven by HCSL clock, is refclk of XIO2001 a NRZ signal?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello-
Typically, an HCSL clock driver would need 50-ohm terminations to GND near the driver outputs. Series resistors (e.g. 33 ohms) may be used to slow down the edges. Figure 19 of the LMK00334 datasheet provides an example interface.
I don't quite understand your second question. An HCSL clock source would drive the XIO2001 RefCLK inputs.
Regards,
Davor