Part Number: TPD4E1U06
Hi,
I am planning to use TPD4E1U06 for ESD protection(EC 61000-4-2, Level 4) on a single USB 2.0 port.
In TPD4E1U06, D+ is connected to Pin 1 and D- is connected to Pin 4.
I want to protect the Vbus line also from ESD. I have not seen any design where in Vbus is connected to Pin 3 or 6 in the IC.
Can I connect Vbus to Pin 3 or 6 for ESD protection? Why/Why not? (I know I can always connect Vbus to a separate TVS diode, but question is specific to connecting Vbus to an input port of the TPD4E1U06.)