Part Number: DP83640
Hello,
My customer is looking to do a reverse loopback to test the Ethernet link between two 10/100 systems using the DP83640.
They are setting register 0x17 bit 8 PMD_LOOP to do this.
Where in the PHY does the loopback occur?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83640
Hello,
My customer is looking to do a reverse loopback to test the Ethernet link between two 10/100 systems using the DP83640.
They are setting register 0x17 bit 8 PMD_LOOP to do this.
Where in the PHY does the loopback occur?
Hi Ivan,
The reverse loopback occurs at the internal MII block of the PHY.
Regards,
Justin