Part Number: TCA9406
Hi Team,
As title, can TCA9406 be used as an SMbus on-off control switch?
Thanks!
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When the OE pin is pulled low, the A and B sides are disconnected. The internal 10 kΩ pull-up resistors also are disconnected, which might or might not be what you want.
If no level shifting is needed, a two-channel switch would be simpler and cheaper.