Part Number: DS64BR111
Hi TI,
I think I found a more suitable repeater for running 1.25Gbps SGMII in the DS64BR111.
I had some quick questions for you though:
- Do you agree that this part should work as well? Should I be able to run it using just the input pins for configuration or do I need an EEPROM or I2C for this lower data rate?
- Is the rise time adjustable? I thought reduction might be better for the longer bit time. Doesn't look like it though.
- Any recommendations for XMT pre-emphasis/RCV CTLE at this lower data rate? We are running through 6 meters of cable.
- I did not understand how the XMT Vcommon mode could vary between 0 to 1.9v (datasheet pg. 7). How is this possible?
- I don't understand what RCV VTX (datasheet pg. 6) is (0.19 to 1.6v). Is this min./max. differential voltage allowed at the receiver?
Thanks Very Much,
Ned