This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: Can sn65dsi86 support panel without HSync and VSync?

Part Number: SN65DSI86

Hi Team,

As title, can sn65dsi86 support panel without HSync and VSync?

Any spec we need to provide to verify ?

Shaq.

  • Shaq

    The DSI specification timing events can be provided in one of two types: Sync Pulses, and Sync Events. The DSI86 both types. For the Sync Pulse type of timing event, the GPU will send VSYNC START (VSS), VSYNC END (VSE), HSYNC START (HSS), and HSYNC END (HSE) packets. For Sync Event type, the GPU will only send the sync start packets (VSS and HSS). For both types of timing events, the DSIx6 will use the values programmed into the Video Registers to determine the sync end events (VSE and HSE).

    Thanks

    David