Part Number: SN65DSI86
Other Parts Discussed in Thread: TEST2
Hello
We are using the SN65DSI86 bridge and the set up that we are working with is the next:
Processor -> DSI to DP bridge -> USB-C connector -> USB-C to HDMI adapter -> HDMI monitor
Our first circuit revision had the TEST2 pin tied directly to ground so we worked with an USB-C to HDMI adapter that was ASSR compatible to get video transmission, now our newest board revision has the TEST2 pin pulled high to make the ASSR feature selectable, until this point the driver source code has not been modified.
After performing some tests with our new board we noticed that the previously described setup reports a link training failure, we thought that with the pull up on the TEST2 pin the original behavior wouldn’t change and only if it was necessary the ASSR settings could be overridden.
With the TEST2 pin pulled high is there any additional settings needed to keep the ASSR compatibility?
Thanks,
Esteban V.