Other Parts Discussed in Thread: TUSB2077A
I am thinking about using this chip in my Fixture design to be able to talk to 14 FTDI Chips.
I have a few questions
1). Are there any layout considerations regarding distances between this chip and upstream/downstream USB ports?
2). Any recommendations for Trace width etc?
3). since I have to communicate to 14 Targets I am planning to use three of these chips in cascaded mode giving me 19 targets. Do I need to use 27 Ohm resistor with 22 pF caps (as suggested in recommended design) at the input of second and third stage of cascaded TUSB2077 chips?
My application requires atleast 5 GPIO and 1 serial port communication capability per target, due to this I have been using FTDI FT232RL chips. in order to simplify my fixture to have less cables (reduce 14 USB cables down to one) I need to go to this chip design. I am open to consider any device/chip that will further reduce the complexity of my circuit.
Thanks in advance
Atif Bhatti