This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB211-Q1: topology of placement check

Part Number: TUSB211-Q1
Other Parts Discussed in Thread: TUSB212

Hi Sir,

Below is the topology of TUSB211-Q1 need consult with you that it will work or not?

And I had checked with customer that move the TUSB211-Q1 to FIO board but it can't work due to there is no spacing for it.

Customer is worry about the trace length is too long before USB2.0 Redriver,

Please help to reconfirm it.

If the trace length out of the design rule, customer will put another redriver between USB MUX and BMC, please help to check if any concern.

Below is the insertion loss information,

BMC---2.4dB @240M (21.5” PCB+MUX+0.5”PCB) ---USB2 Redriver --- 1.9dB@240M (0.5”PCB+FFC cable+1”PCB+ Type-A Connector) --- Type-A Connector.