Part Number: TCAN1042HG-Q1
Other Parts Discussed in Thread: TCAN1042V-Q1, TCAN1042-Q1
Hi All,
Currently my customer is using TCAN1042V-Q1 (TCAN1042HVDRBRQ1) with "V suffix" that is with integrated level shifters.
He would like to replace on another board the SN65HVD251D / SO8 with the transceiver TCAN1042-Q1 but, having the first only the VCC (5V), I would need the version without level shifters (without V suffix, ie TCAN1042HGDRBTQ1) so that I can replace the second to the first without changes.
Can you please confirm that the variants with and without V have the same characteristics, as it seems from the datasheet?
Many Thanks,
Antonio