Part Number: TUSB320
Other Parts Discussed in Thread: BQ25890, , TPS25910
Dear TI Team ,
I will apreciate if you can check if the circuit is functioning properly with the USB Type C connector standards please. I am kinda confused on how to proceed at some points .
My aim is to configure the port of USB C in DRP mode .
I have attached a scheme which shows the flow chart of the Power Multiplexer section.
In the system design , there are 3 source of input available. I have an Aux input connector which is 5V0_in , Vsys _Backup (4.4Volts) output from BQ25890 Battery Charge Management IC , 5 Volt Dc Power that can be fed from the connected USB C connector , 5V_USB.
Question 1, is the below scenario working for DRP?
When a host is connected at USB C connector , we have the TUSB320 detecting CC lines , getting TUSB_ID LOW and TPS25910 drives 5 Volts with MAx 3A to the host if there is power available in the AUX connector which is 5V0_in.
At this point Do I have to also send the TUSB_ID signal from TUSB320 to the ATSAMV71Q21Processor?
If the Aux Power is not available in Aux connector, The BQ25890 will start powering the VCC_P5v0 net from the mosfet IC6 IRLML6402.
Question 2,
Should i also send power up to Connected USB Host with the 4.4 volts output from BQ25890 when there is no Aux Power available?
Question 3 ,
Are the schottky diodes U11-U12 positioned properly for the DRP mode and the power scenarios explained above?