This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9406: Use a TCA9406 with multiple I2C devices

Part Number: TCA9406
Other Parts Discussed in Thread: INA260, PCA9306

Hi,

I need to add a 1.8V slave to my design. After looking for an I2C level translator, TCA9406 seems to be a good candidate for the job however I'm little confuse whether it is able to upper the voltage from VCCA to VCCB or lower from VCCA to VCCB.

This is how I think it should be used. ESP32 is a I2C master while INA260 and ICM-20948 are both slaves. INA260 at 3.3V and ICM-20948 at 1.8V.

Is it ok?

Thank you